Where to buy a step down transformer in Berlin?

Dear community members,
I brought my Bravia KDL-52XBR2 TV and Onkyo TX-SR805 receiver from the US. Apparrently, Onkyo will work at 120 V only, Bravia manual says 120-240 V but I also do not want to risk just plugging it in. In any case, I need a step down transformer at least for the receiver. There are some available at Amazon site but I would prefer to buy locally. Any pointers will be much appreciated.
Also, if someone could confirm if indeed it is safe to plug in the TV as is (no information on the back panel).
0
Anmelden oder Registrieren, um zu kommentieren.
Antworten
Hi @Mathim, if the Bravia KDL-52XBR2 TV can be operated with 120-240 V, it should be safe to plug it in directly using a simple travel adapter such as Brennenstuhl 1508520 Reiseadapter, available at our Berlin Kreuzberg Store. As for the converter, we could offer the VOLTCRAFT AT-400 NV 400 W 240 V/AC (400 Watt max.), which could be ordered online for pick up on May 31st./ June 1st.